STLINK-V3SET SWD Programming not working with TAG connector on STM32G474E-EVAL1
Hi, Im having issues programming with the STLINK-V3SET on the STM32G474E-EVAL1 board with the tag connector(CN15) I get the following output when using the STM32CubeProgrammer
13:09:01 : UR connection mode is defined with the HWrst reset mode
13:09:01 : UR connection mode is defined with the HWrst reset mode
13:09:01 : ST-LINK SN : 0039002B3234510836303532
13:09:01 : ST-LINK FW : V3J16M8B5S1
13:09:01 : Board : STLINK-V3SET
13:09:01 : Voltage : 0.64V
13:09:01 : Error: Unable to get core ID
13:09:01 : Error: No STM32 target found! If your product embeds Debug Authentication, please perform a discovery using Debug Authentication
And with programming with the IDE I get the following output
Starting server with the following options:
Persistent Mode : Disabled
LogFile Name : C:\Users\aiglesias\Documents\test\Debug\st-link_gdbserver_log.txt
Logging Level : 31
Listen Port Number : 61234
Status Refresh Delay : 15s
Verbose Mode : Enabled
SWD Debug : Enabled
InitWhile : Enabled
Error in initializing ST-LINK device.
Reason: No device found on target.
I have no issues programming with the JTAG or STDC14 connectors on the board. Im using the USB cable that came with the board to power it.