stm32 ADC scann mdoe
In the ADC scan mode in STM32 microcontrollers, the digitized value of all input channels is dumped into ADCx->DR. Is there a register or flags to find out which ADC channel the data currently in the ADCx->DR register
```
void HAL_ADC_ConvCpltCallback(ADC_HandleTypeDef* hadc)
{
if(hadc->Instance == ADC1)
{
uint16_t adc_data;
// Read the converted data from the ADC data register
adc_data = ADC1->DR; //I don't know which ADC channel this data is related to
// Process the ADC data as needed
// ...
}
}
void ADC_Init()
{
ADC_ChannelConfTypeDef sConfig;
hadc.Instance = ADC1;
hadc.Init.ScanConvMode = ENABLE;
hadc.Init.ContinuousConvMode = ENABLE;
hadc.Init.NbrOfConversion = 2; // Number of channels to convert
hadc.Init.DiscontinuousConvMode = DISABLE;
hadc.Init.ExternalTrigConv = ADC_SOFTWARE_START;
hadc.Init.DataAlign = ADC_DATAALIGN_RIGHT;
hadc.Init.NbrOfDiscConversion = 1;
if (HAL_ADC_Init(&hadc) != HAL_OK)
{
Error_Handler();
}
// Configure the ADC channels to be converted
sConfig.Channel = ADC_CHANNEL_0;
sConfig.Rank = 1;
sConfig.SamplingTime = ADC_SAMPLETIME_13CYCLES_5;
if (HAL_ADC_ConfigChannel(&hadc, &sConfig) != HAL_OK)
{
Error_Handler();
}
sConfig.Channel = ADC_CHANNEL_1;
sConfig.Rank = 2;
if (HAL_ADC_ConfigChannel(&hadc, &sConfig) != HAL_OK)
{
Error_Handler();
}
}