STM32 Custom Board: No Target STM32 Found in STM32CubeProgrammer
I created a custom STM32 board for a motor controller, but I am having trouble even programming it using the STLink V2. I am using the STM32C071KBT6N MCU that I purchased from Mouser. I soldered it onto my board using drag soldering. I soldered other components near it with hot air.
I have tried to power the board through an external 3.3V power supply and through the STLink itself.






This STM32 model has the same pin for PA14-BOOT0 and SWCLK. But I just directly connected the pin to the header for STLink V2.
I also do not have an external crystal oscillator to connect because I wanted to keep it simple and just use the internal clock.

I get this error in STM32 Cube Programmer.

And these are the settings I am currently using.
I have tried different combinations of settings and have held the reset button down, but I still end up with the same error.
I am not sure if something is wrong with my design, the chip that I received was bad, or I somehow destroyed the chip while soldering.
I hope someone can help me. Thanks!