STM32 fails to connect if AREF is not connected to VDD
Hi, I'm new in the STM32 world. I recently bougth the STM32L031K6 nucleo board and I am doing a project where I need to connect the analog reference to a voltage different from VDD. So I de-soldered the solder bridge that connects AREF to VDD (SB10). Now if I plug the cable in I get a fail file that says: "The interface firmware FAILED to reset/halt the target MCU" and the board doesn't work, if I connect vcc to aref all works good. What could it be?
Thank you all!