Skip to main content
Graduate
April 13, 2025
Solved

STM32 MCU discovery kit

  • April 13, 2025
  • 2 replies
  • 438 views

Hi All,

I search for STM32 MCU discovery kit which meets the following conditions.

・It have a 4-inch or larger LCD screen.

・It have 10 or more GPIO ports that user can use freely.

・It have 2 or more UART ports that user can use freely.

STM32U5G9J-DK2 have 16 GPIO ports, but only have 1 UART according to user manual.

Is there anything else that meets the above conditions.

Thanks in advance.

    This topic has been closed for replies.
    Best answer by Tesla DeLorean

    Not sure

    Most have pins all well used up.

    There's perhaps a couple of the F7 and H7 with screens, and Arduino Shield headers exposing GPIO / UART

    Perhaps some NUCLEO-144 you can mount a display too? Riverdi had a board as I recall.

    Other than that you might need to look up some third-party boards

     

    2 replies

    Graduate II
    April 14, 2025

    Not sure

    Most have pins all well used up.

    There's perhaps a couple of the F7 and H7 with screens, and Arduino Shield headers exposing GPIO / UART

    Perhaps some NUCLEO-144 you can mount a display too? Riverdi had a board as I recall.

    Other than that you might need to look up some third-party boards

     

    Super User
    April 14, 2025

    The STM32H747I-DISCO has all of those.

    PC6/PC7 are free for USART6

    PD5/PD6 are free for USART2