Question
STM32 Nucleo32 Dev Board I/O Current Limit
Are the STM32 Nucleo-32 dev boards IO pins rated for 50mA? I couldn't find any information about the max ratings of the IO pins for the dev boards. I need them to be rated to up to 5V, and be able to output 50mA of current.
If this is not possible, would someone be able to recommend an MCU that is able to do this but is around the size of an arduino nano?
Thank you for the help!