STM32 overheating when SMBUS device connected
I am using a STM32L4R9ZGJ6 that has the following issue: When it is powered up and a SMBUS slave device is connected, the CLK line over heats and destroys the processor.
This is the device we are plugging into the board:

This is the STM32 with the CLK and DATA lines shown on PB6 and PB7:

What could be happening that causes the processor to fail? Immediately upon plugin the STM32 gets red hot and burns.