STM32CubeIDE + STLINK-V3MINI + NUCLEO-L496ZG
I'm running a STM32L496ZGT6U on a NUCLEO-L496ZG. Previously, I used the NUCLEO's integrated ST-LINK/V2-1 debugger/programmer. Now, I have sawed off the ST-LINK part of the PCB. I want to program and debug using a STLINK-V3MINI.
I wired up STDC14 for STLINK-V3MINI (STM32 JTAG/SWD and VCP) to the NUCLEO:
(Web page)
I'm powering the NUCLEO board with 9.0 V on Vin.
If I connect a USB cable to the V3MINI and try to debug in STM32CubeIDE, I get:
STMicroelectronics ST-LINK GDB server. Version 7.1.0
Copyright (c) 2022, STMicroelectronics. All rights reserved.
Starting server with the following options:
Persistent Mode : Disabled
Logging Level : 1
Listen Port Number : 61234
Status Refresh Delay : 15s
Verbose Mode : Disabled
SWD Debug : Enabled
InitWhile : Enabled
Target no device found
Error in initializing ST-LINK device.
Reason: No device found on target.Error in final launch sequence:
Failed to execute MI command:
target remote localhost:61234
Error message from debugger back end:
localhost:61234: Connection timed out.
Failed to execute MI command:
target remote localhost:61234
Error message from debugger back end:
localhost:61234: Connection timed out.
localhost:61234: Connection timed out.If I go to Debug Configurations, Debugger, ST-LINK S/N, Scan, it finds 003800194741500820383733.
If I go to Windows Device Manager, Ports (COM & LPT), I see one entry: STMicroelectronics STLink Virtual COM Port (COM7). If I bring up PuTTY, I can connect to that port and interact with the last program that I flashed into the device.
Should I be able to make this work? I have never used the STLINK-V3MINI before.
STLINK-V3MINI LKV3MINI$AT2
MB1467-V3MINI-B02 A213402626
MB1467B9
STM32CubeIDE
Version: 1.11.0
Build: 13638_20221122_1308 (UTC)
I also went to https://www.st.com/en/development-tools/stsw-link009.html and (re)installed the ST-LINK, ST-LINK/V2, ST-LINK/V2-1, STLINK-V3 USB driver for Windows, but it didn't make any difference.