STM32Cubemonitor-UCPD "send free text"
Hi STMicroelectronics Team,
I'm using a STEVAL-2STPD01 USB PD Board with STM32G071RBT6 NUCLEO-G071RB controller board. I'm using it in a Source Mode.
I'm trying to get the Input Power value (field = "send free text") which was entered in the STM32Cubemonitor-UCPD software out of the software so that I can set the USB Sink according to the input power (since it is having an option of power sharing between the two USB type-c ports).
Since the Source Capabilities at the two Type-C sink port depends on the Input power, this information is required.
Can you guys help me, how can I get that value out of the software (STM32Cubemonitor-UCPD).
Yes. I know that I can be able to see that information in Trace window, But I want to extract that information from software to process it externally.
Regards,
Mohan Krishna N D