STM32CubeProgrammer works fine with NUCLEO STM32F767ZI but fails to find NUCLEO STM32F446RE.
Hi, I have 2 Nucleo boards: NUCLEO STM32F767ZI (F4) and NUCLEO STM32F446RE (F7).
I'm using macOS 10.15.4 omn MacBook Pro 2017 with STM32CubeProgrammer 2.4.0 and stlink tools from brew (GitHub.com/texane/stlib).
When I plug in F4 over USB-C to USB-Mini then neither Cube Programmer or stlink command line tool can find it. The device is powered properly and begins the blinking demo.
But when I use F7 over USB-C to USB-Micro then both tools properly identify the board and the IC and I can program it over built-in ST-LINK.
So would anyone know what might be the issue with F4? Am I using wrong cable (unfortunately it's the only one I have) or maybe do I need to do anything with the jumpers? I just took both boards from their boxes and plugged them in. And as described F7 works fine, but F4 is not discoverable...
Any help would be appreciated. Many thanks.