STM32F072C8T6 - Device not found - struggling!
Hi,
I am working with STM32F103 and STM32F072. The first one (103) works very well without any problem. The second one (072) does not work.
I'm using the stlinkv2, connected via SWD to my board (schematic is correct).
BOOT0 pin is tied to gnd with a resistor. The reset occurs once I press debug on stmcubeIDE but it can not find the device.
Why did it find without problem the stm32f103 and not the 072?
What can be the problem? The boot0, reset and supply management are both the same!
Thanks.
Edit:
Error in initializing ST-LINK device.
Reason: No device found on target.