STM32F072C8T7 needs hardware reset upon power on to work!
When the device is connected to the ST_LINK, after firmware upload, it works perfectly fine. When I remove the ST_Link and then turn OFF and ON my device, it does not work, unless I initiate a hard reset.
Also, the device works fine when I chose the internal oscillators as a clock source (both with ST-Link connected and without it).
The problem only persists, when in the clock configuration, I choose the clock source and the HSE (external 8MHZ crystal oscillator). The Boot0 pin is pulled low using a 10K resistor. The reset IC keeps the NRST low for at least 300ms as it should be according to the datasheet.
I have used the same 3.3V rail for both the VDDA and VDD. I think this is causing the issue.