Skip to main content
Graduate
November 25, 2019
Question

stm32f09 command line programming issue

  • November 25, 2019
  • 0 replies
  • 546 views

issue-when programming using the Command line utility it indicates success but the unit does not boot.  when programming from the GUI the unit powers up correctly.  I used the same command line on an st32f07 without issue.  Here is the command line.​  start /B/wait st-link_cli.exe -c SWD UR -ME -P c:\RF6_RP_FAC_1.5.bin 0x8000000.  Am I missing a setting/command?  I attached a screen shot of the firmware in the stlink programming utility

    This topic has been closed for replies.