Skip to main content
Explorer
August 1, 2016
Question

STM32F0Discovery STLINK Virtual Comm Port

  • August 1, 2016
  • 1 reply
  • 710 views
Posted on August 01, 2016 at 19:12

The STM32F0Discovery (board MB1034B) has a connection between the STM32F103 used for the STLINK and USART1 of the STM32F051.  It seems like this connection is intended for use as a USART comm port between the STLINK and the F0 processor.  

Is there a version of the STLINK firmware that enables this link?  I downloaded the latest STLINK firmware from ST-LINK v3.8.0 (reported to be V2.J25.S0 STM32 Debugger) but I don't have a COMM port assigned to the ST-LINK.

(Yes, I have shorted SB14 and SB15 so as to physically connect the signals to the STM32F103)

#stlink-stm32f0discovery-vcp
    This topic has been closed for replies.

    1 reply

    Graduate II
    August 1, 2016
    Posted on August 01, 2016 at 20:17

    This functionality is not supported on your board.

    The boards supporting the VCP and mbed have a higher grade F103 part, and the update tool contains different firmwares for the assorted models. Some of the DISCO boards have been reissued as DISC1 models that support mbed.