Skip to main content
Visitor II
July 15, 2020
Question

STM32F103 random reset

  • July 15, 2020
  • 1 reply
  • 995 views

Hello, we have made a 2 layer board for a STM32f103, and apparently it works fine but we get a random resets now and then. When that occurs there is a 1 in the Bit 27 PORRSTF: POR/PDR reset flag and Bit 26 PINRSTF: PIN reset flag of the Control/status register (RCC_CSR). I think it might be some kind of noise on that trace? Attached is a picture of that portion of the PCB and SCH, with the RESET trace highlighted.

Any ideas of what could be the error?0693W000001syI7QAI.jpg0693W000001syICQAY.jpg

    This topic has been closed for replies.

    1 reply

    Super User
    July 15, 2020

    All reference designs have NRST bypassed to GND with a 0.1uF capacitor to prevent spurious resets. Yours doesn't have a cap at all. I would suggest adding that to see if it fixes the problem.