STM32F103C8T6 Blue Pill project
First and foremost, as of this point I know virtually nothing about these MC's but through this project, I'm hoping to learn. What I'd like to get some assistance on is just a few basic pointers and perhaps direction so that I'm not chasing my tail.
The project is to enable an instrument cluster from a slightly newer vehicle (2003) be used in a slightly older vehicle (2002). Most of the gauges will work by simply re-pinning the connector, but there are 2 gauges that require a PCM swap and tuning to get working, the volts gauge and the oil pressure gauge. As best I can tell, both the 2002 and 2003 rely on Class 2 serial data, interpreted by the PCM, to feed these 2 gauges. So I want to bypass the PCM, have this data from sensors feed into this hypothetical module I want to build, which will then correctly display the data I want to see on these 2 gauges.
I hope this clearly explains the goal and the hurdle that exists. So what I'd like some input on specifically is how best to go about setting up my environment for this. I've located a STM32 dev board (for which this post is titled) and USB to UART programmer, but I'm thinking I also need a suitable voltage regulator to ensure proper voltage is maintained for this dev board, among other things. Or if even there are some good resources for the foundations of what I'm wanting to do, I think even that would be very beneficial. I'm coming from a background of database development, so aspects of coding logic are pretty familiar, I just have no idea where to start here. Thanks!