STM32F103C8Txxx custom board, glitches after few seconds
Hello everybody,
I made for school a custom stm32f103C8Txxx board.
Programming with a ST-Link V2 work without a problem.
To test the pcb, there are 2 led's (pin pc13 en pa10), they both illuminate every 500ms (easy code to test functionality).
The code wil run, for a few seconds and then glitches and does not respond... even after reset, it will glitch instantly.
If I dissconnect power for a minute, it will work again, but only for a few seconds and then glitches again.
Any ideas what it could be?
I added the schematic for everyone to see (don't mind the usb-c stuff, those components are not place on the pcb)
Edit 1:
Boot 0 and Boot 1 are determined with jumpers. Some parts of the schematic are based on the blue pill.