Question
STM32F4 Hardware for external clock
I want to develop my own PCB using STM32F4. I want to use one external clock (16 MHz). I wonder where I have to connect the clock: OSCIN32-OSCOUT32 (pins 3 and 4) or OSCIN-OSCOUT (HSE) (pins 5 and 6 in STM32F446RET).
I can see in the development board's schematic how there is an empty footprint for X3 (pins 5 and 6) and I don't know if it is using the debugger's clock.
Thanks in advance.