Skip to main content
Visitor II
November 10, 2020
Question

STM32F407VG --- I2C Flag error

  • November 10, 2020
  • 0 replies
  • 684 views

I have coded a program for I2C for my STM32F407 DISC-1 board.

In which STM32 acts as master and sends data to a Arduino UNO whenever user button on STM board is pressed

code works fine , i am getting proper output which is expected but when I run code as a whole .

but when i was doing step wise debugging, their is some strange behavior

after sending the address the ADDR bit is set (signifying the address matches the slave)

0693W000005As7zQAC.pngthen when i go to the function to check ADDR bit to proceed further the ADDR bit resets 

0693W000005As7uQAC.png 

why is this happing i have only switch to a different function to check the bit , i haven't even read the register or do masking to get the bit value .

and as per reference manual ADDR bit resets when we read SR1 followed by reading SR2

but if run the code without stepwise debugging it runs fine , so code is fine

then why this is happing in stepwise debugging , is this because of some ST-Link debugger , or anything else ?

I am using STM32F407 DISC-1 , on board debugger.

    This topic has been closed for replies.