(STM32F411CE) Always in system bootloader when powering on
I have a custom board which always enters the DFU USB system bootloader when powering on, even though BOOT0 & BOOT1 pins are driven to ground. After I load a simple test program on it (via dfu-util), it runs the program just fine. However, when I remove power, it ends up back in the bootloader when I power it back on.
I've attached the schematic. It's based on another board design which works just fine.
I feel at a lost for why this could be happening. I've read the datasheet and the bootloader application note (AN2606). I've tested that the BOOT0 & BOOT1 pins are connected to ground. Is there another way that the chip could automatically go to the booloader and not execute the user program on power-up?
Thank you!