STM32F446 Nucleo won't boot on external power
I have a project, using a Nucleo board, the software runs fine when powered by the USB cable, but when I use an external 12v PSU connected to the external input, on power-up, it does not start. Pressing the reset button makes everything start as expected. Unfortunately, I do not have an oscilloscope to look at the power-line as it is starting. I have tried an external power monitor to reset the card, but this did not work either, I am happy that this external monitor was working as removing it's power & re-applying caused the expected reset.
Other than changing the link for the power from USB to external, I have not changed anything else on the Nucelo board.
Has anyone got any suggestions as to what I have missed?