Skip to main content
Visitor II
October 11, 2016
Question

STM32F769I Disco board image file Issue

  • October 11, 2016
  • 5 replies
  • 1405 views
Posted on October 11, 2016 at 13:37

Hi,

Recently I bought STM32f769I DISCO Board and power the board via USB, it work fine.

I trying to flash the new image file from ST website that new image file was flashed and working. 

Now, trying to change old image file (Pre-installed image file) which comes with STM32f769I DISCO board. then I searched in ST website found one STM32Cube_FW_F7_V1.4.0 image file and flashed into STM32f769I DISCO board. but the GUI was not same as old image file(Pre-installed image file).

Please help me where I get old image file(Pre-installed image file) for STM32f769I DISCO board.

#stm32f769i-disco-board #stm32f769i-disco-board #st-link/v2-in-circuit-debugger
    This topic has been closed for replies.

    5 replies

    Technical Moderator
    October 11, 2016
    Posted on October 11, 2016 at 15:19

    Hi kamatchi.thangaraj,

    The package STM32Cube_FW_F7_V1.4.0  contains various examples.

    You should look to the demonstration available under STM32Cube_FW_F7_V1.4.0\Projects\STM32F769I-Discovery\Demonstration.

    -Mayla-

    Visitor II
    October 12, 2016
    Posted on October 12, 2016 at 12:13

    Hi Mayla,

    Thank for your Response,

    As you mentioned  STM32Cube_FW_F7_V1.4.0\Projects\STM32F769I-Discovery\Demonstration working, but it's not new image file(pre-installed STM32F769INH DISCO board GUI)  it looks like STM32F746G  GUI !!!.

    But we need switch STM32F769INH DISCO board GUI and Firmware.

    Please kindly support to resolve this issue.

    Technical Moderator
    October 14, 2016
    Posted on October 14, 2016 at 17:03

    Under the folder  STM32Cube_FW_F7_V1.4.0\Projects\STM32F769I-Discovery\Demonstration\Binary, you find 2 hex files:

    - STM32CubeDemo_STM32769I-DISCO_V1.0.1.hex

    - STM32769I-DISCO_DEMO_V1.0.0_FULL.hex

    STM32769I-DISCO_DEMO_V1.0.0_FULL.hex is the pre-installed image provided as demonstration.

    In the package release note, you find this note: 

    Demonstrations Firmware for STM32F7x9I_EVAL and STM32F769I-Discovery, provided within this package, don't embed:

     

    - TouchGFX demonstration module. Free evaluation version of the TouchGFX demonstration, based on Draupner Graphics’ commercial graphic library, is available at www.touchgfx.com/stmicroelectronics

     

    - Embedded Wizard demonstration module. Free evaluation version of the TARA Systems demonstration, is available at www.embedded-wizard.de/stm32

    -Mayla-

    Visitor II
    November 8, 2016
    Posted on November 08, 2016 at 11:04

    Hi,

    We have gone through website and in the support devices for ST-LINK/V2 in-circuit Debugger/Programmer STM32f7 Series Micro-Controller is not mentioned.

    We would like to know whether ST-LINK/V2 in-circuit Debugger/Programmer Support STM32f7 Series Micro-Controller?

    Thanks and Regards,

    K.Thangaraj
    Visitor II
    November 8, 2016
    Posted on November 08, 2016 at 13:40

    Yes,

    this should be possible. When you take a look on some F7 nucleo boards, the ST-Link is present there as well, version 2-1. But the version should be only matter of firmware, which is upgradable...

    Have a nice day,

    Renegade