STM32F769I-Disco - no ST-Link detected
Hi guys,
I am new to STM32F769I-Disco and I‘ve got an error by trying to connect the STM to my pc.
In the STM32CubeIDE 1.4.0 I got the message: No-ST-Link detected
In ST-Link-Utility i got the same message.
ST-Link-Utility -> about: ST-Link-utility: v4.5.0; USBDriver.dll v5.1.2; ST-Link cli v3.5.
Additionaly no USB-Device is shown in my device-manger and the LD8(ST-Link connection) is blinking red. The display and so on is working well. I powered the board with usbhs and LD5 is green and LD6 is red.
Before I have worked with the same pc with STM32L0 and F1and both are ok. I’m able to connect in the IDE and in ST-Link-Utilities.
The ST-Link Debug version is 2.1.0.0.
I dont know what goes wrong.. I changed the usb cables and ports but no success.
Does anyone have an idea where the problem is ?