STM32F777 1.125 Volt on VCAP
Is this a normal reading?
Havent installed ALL caps yet. I think I had bad contatc between SWCLK and connector, could this have caused it not to be recognized by cubeprogrammer?
I had a F2 with 1.188 volt wich I could program, communicate with via programmercube
Now my stomahc is aching and I AM WEAK IN THE KNEES. Almost feel like passing out.
This one I couldnt program yet, but will check a few things.
Its 216 BGA on a custom board, I can see that I'm aligned judging from the vcaps, since 2 tiny islands underneat are at 1.125 and the bga is well flattened.
I have VDDA connected obviously.
Bypass reg grounded directly
PDR on VCC directly.
VDDDSI physically connected to VCAPDSI because I dont use.
BOOT0, BOOT1 pulled down
NRST pulled up and connected to debugger mini cortex header.
What else?