Skip to main content
Visitor II
August 26, 2022
Solved

STM32F779AI WLCSP 180 pins package layout examples

  • August 26, 2022
  • 2 replies
  • 1614 views

I would like to use the STM32F779AI, in WLCSP package. I did not find any application notes, or schematics or dev board for such MCU.

Is there some litterature or example, schematics, ... talking about layout rules, VIAs, etc... for the WLCSP-180 (pitch 0.4mm) package.

Thanks in advance

Pascal

    This topic has been closed for replies.
    Best answer by FBL

    Hi @pazcal​ 

    Refer to this application note Getting started with STM32F7 Series MCU hardware development section 6.7 Recommendations for the WLCSP180 package then 8.5 WLCSP143 0.4 mm pitch design example

    Also you can check the datasheet section 3 for more details about the pinout and package characteristics

    2 replies

    Graduate II
    August 26, 2022

    TBH I think the people you should start with are the PCBA guys you work with, they'll have a lot more insight into the board, stack-up, solder mask, and via-in-pad type stuff they can work with, and which PCB vendors do a good job of fill/planarization, etc.

    pazcalAuthor
    Visitor II
    August 31, 2022

    Thanks for answer, but the question came from the PCBA Guys.

    BR

    paz

    FBLAnswer
    Technical Moderator
    August 29, 2022

    Hi @pazcal​ 

    Refer to this application note Getting started with STM32F7 Series MCU hardware development section 6.7 Recommendations for the WLCSP180 package then 8.5 WLCSP143 0.4 mm pitch design example

    Also you can check the datasheet section 3 for more details about the pinout and package characteristics

    pazcalAuthor
    Visitor II
    August 31, 2022

    Thanks for your answer. The A.N will help

    BR

    paz