Skip to main content
Visitor II
February 14, 2020
Question

STM32G030F6P6 Running at 2.5V - Can I use STLINK-V3SET in SWD Mode?

  • February 14, 2020
  • 0 replies
  • 436 views

I have designed a prototype based on the STM32G030F6P6  microcontroller. The microcontroller runs on a battery. The power to the microcontroller comes from a 2.5V regulator. Is it possible to debug this configuration using an STLINK-V3SET in SWD mode? The manual seems to indicate that the minimum voltage is 3V. Any suggestions?

Thank you,

Max

    This topic has been closed for replies.