Skip to main content
Visitor II
July 28, 2020
Question

STM32G071RBT6(Reason : (4)No device found on target.)

  • July 28, 2020
  • 3 replies
  • 1106 views

Hello,

I have the following problem when using the Nucleo board.

I do not have a mini-usb.

So I use to ST-LINK.

However, the following warning message is displayed.

Please tell me the solution.

Thank you for reading.

※ I use to STM32CubeIED.

0693W000003BUZzQAO.png0693W000003BUXeQAO.jpg

    This topic has been closed for replies.

    3 replies

    Visitor II
    July 28, 2020

    check that gnd, swdio, swclk lines are correctly shared between stlink and MCU. use a multimeter to check​

    Bryan_KIMAuthor
    Visitor II
    July 29, 2020

    Thank you for the answer.

    I linked it like the datasheet below.

    but it isn't operation.

    CN11

    1 - VCC

    2 - SWCLK

    3 - GND

    4 - SWDIO

    5 - RESET

    0693W000003BZ6IQAW.png

    Graduate II
    July 29, 2020

    That's for OUT-BOUND connectivity.

    Review the schematic, understand the circuit..

    Super User
    July 28, 2020

    Check you power supply. I would suggest connecting to VIN not VDD directly.

    Bryan_KIMAuthor
    Visitor II
    July 29, 2020

    Thank you for the answer.

    I linked it like the datasheet below.

    but it isn't operation.

    0693W000003BZ5tQAG.png

    Graduate II
    July 29, 2020

    Can't in-bound SWD connection via that header, not how it works.