Skip to main content
Graduate II
August 15, 2023
Question

STM32G0B1RE failed to connect

  • August 15, 2023
  • 1 reply
  • 2165 views

Hi,

My nucleo stm32g0b1re board is failed connect after option byte Boot0 checked in Flash Security.

Tarun_0-1692113644398.png

I've tried many ways to connect board/ease modified SBSFU  on the flash but no luck. could someone help me to recover board?

TIA

    This topic has been closed for replies.

    1 reply

    ST Employee
    August 16, 2023

    Hello @Tarun , 

    If you are unable to connect to your Nucleo STM32G0B1RE board after enabling the Boot0 option byte in Flash Security, it is likely that the board is stuck in bootloader mode. To resolve this issue, you can try the following steps:

    1. Disconnect the board from your computer.
    2. Short the BOOT0 pin to GND using a jumper wire or a switch.
    3. Reconnect the board to your computer and try to connect to it.
    4. If you are able to connect to the board, you can clear the option byte by erasing the chip or using your programming software to clear the option byte.
    5. Once the option byte is cleared, you can remove the jumper wire or switch from the BOOT0 pin and try to connect to the board again.

    Foued

    TarunAuthor
    Graduate II
    August 16, 2023

    Hi Foued,

    I shorted pin 7 and 8 in the image but still same error seen on the Cubeprogrammer.  Is am I missing anything?

    Tarun_1-1692179183392.png

     

     

    TIA

    TarunAuthor
    Graduate II
    August 26, 2023

    Sorry it didn't helps. I have to replace my dev kit.