Skip to main content
Visitor II
August 28, 2020
Question

STM32G474 - Using WLCSP81 package on 1/4 brick power modual

  • August 28, 2020
  • 1 reply
  • 883 views

Dear ST expert,

STM32G474 serials are very good option on digital power control, and I see the WLCSP81 package is pretty small(only 4mmx4mm). I plan to use WLCSP81 package on 1/4 bick power module which is 12 layers and the topology is Hard Switch Full Bridge.

My questions: Is there any risks of using the WLCSP81 package in bick power module? That would prefer if you could provide the information of the conditions/limitations of using WLCSP81 package. From my previous experience, QFN package are commom used in bick module, I'm not sure if WLCSP81could be used in this case.

Thanks

    This topic has been closed for replies.

    1 reply

    ST Employee
    May 27, 2021

    Hi JTan.5 ,

    I think there is no problem. Mechanical properties should be similar: WLCSP package dimensions are ~ 4x4mm and QFN package 7x7mm. Number of balls are much more in WLCSP package (81) with comparison to QFN (48). Then is important the PCB design - temperature cycles on package.

    Regards

    Igor