Skip to main content
Visitor II
January 24, 2025
Solved

STM32H563RG VCAP connection

  • January 24, 2025
  • 1 reply
  • 890 views

For product A (68-pin VFQFN package), pins 31 and 66 are VCAP pins, and 2.2uF capacitors have been placed on each pin. Should pins 33 and 66 be connected to each other, or is it sufficient to place the capacitors on each pin individually?

kimcm2_4-1737700169586.png

 

 

kimcm2_1-1737700058544.png

kimcm2_3-1737700092193.png

 

 

 

    This topic has been closed for replies.
    Best answer by STTwo-32

    Hello @kimcm2 and welcome to the ST Community.

    As you can see on the AN5711

    «  It is recommended to connect the two VCAP pins together. If there are two VCAP pins (such as for the LQFP64 package), each pin must be connected to a 2.2uF (typical) capacitor (for a total approximately 4.4 F) »

    Best Regards.

    STTwo-32

    1 reply

    STTwo-32Answer
    Technical Moderator
    January 24, 2025

    Hello @kimcm2 and welcome to the ST Community.

    As you can see on the AN5711

    «  It is recommended to connect the two VCAP pins together. If there are two VCAP pins (such as for the LQFP64 package), each pin must be connected to a 2.2uF (typical) capacitor (for a total approximately 4.4 F) »

    Best Regards.

    STTwo-32