Skip to main content
Visitor II
October 10, 2024
Question

STM32H573VIT3Q - Vcap pins have no voltage

  • October 10, 2024
  • 2 replies
  • 2363 views

Hello Everyone :)

I have designed a custom board using STM32H573VIT3Q MCU. when I connected it with st link, the st link didn't recognize it.
After I checked the voltages on the power pins, I saw all the power pins were normal except the VCAP pin (not outputing voltage at all..about 50mV).

The Vcap capacitors P.N is (Digikey) : 490-GRM155Z71A225KE01DCT-ND

 

Attached schematic for more information.
Please your help.

(Note, FB1506 is a mistake, and is not assembled). 

 

Thanks alot !

    This topic has been closed for replies.

    2 replies

    Amit_En_CAuthor
    Visitor II
    October 10, 2024

    Update:

     

    1. I disconnected R1502.

    2. Assembled R1501.

    3. Assembled L1500.

     

    In other words - I choose the SMPS mode. (instead of the LDO).
    Works like a charm.

     

    If anyone has an idea why the LDO mode didn't work - please your advice (To help people who will have same question in the future ;)

    Thanks,

    Amit.

     

     

    Technical Moderator
    October 10, 2024

    Hello @Amit_En_C  and welcome to the Community;

     

    Could you please refer to AN5711 precisely Figure 5. STM32H563/H573 power-supply scheme with SMPS and Figure 16. STM32H573 reference design (SMPS example) and check your schematic. Are you use an L1=2.2µH between VLXSMPS and Vcap, it is Required for SMPS packages on VLXSMPS pin.

    KDJEM1_0-1728576114324.png

    KDJEM1_1-1728576235741.png

    KDJEM1_2-1728576582530.png

    Note: It is recommended to connect the two VCAP pins together.
    It is recommended to use a large plane VCAP and connect the SMPS pin to the VCAP plane with a large wire
    (as the total power is flowing through this wire). Then, put the 100nF ceramic capacitor on each VCAP (as close
    as possible to the VCAP ball) and add the 4.7uF on each VCAP ball.

     

    I hope this help you!

    Thank you.

    Kaouthar

     

     

     

     

     

    Amit_En_CAuthor
    Visitor II
    October 20, 2024

    Hi KDJEM.1

     

    Thanks for your comment, but your answer was about SMPS mode.

    My problem was not about the SMPS mode. (SMPS worked fine)

    My problem was related to the LDO mode. (LDO didnt wake up... there was no voltage on Vcap), and because of that issue, I had no choise but to use the SMPS mode.


    Thanks,

    Amit.

     

    Technical Moderator
    October 20, 2024

    Dear @Amit_En_C ,

    This is an expected behavior as you have an MCU reference supporting only SMPS. Which is ending by Q. To have LDO you need the part without Q at the end . This option is exclusive and not inclusive and hard coded out from our factory .

    IMG_0100.jpeg

    Hope it helps you 

    STOne-32