STM32H725 SMPS Issue
Hello,
I designed a motor controller with an STM32H725ZG, and I am having problems with
the SMPS. First, with the board just assembled, the stm32CubeIDE let me upload
a simple code (activating 25MHz crystal, debug, and blinking a led) one time.
After uploading it, the debugger shows "Target not found..."
"Shutting down..." and it can't be programmed never again. After some
measures I realized that the SPMS is throwing 0.06V, so I decided to bypass the
VDDLDO to 3V3 and after that it works perfectly.
Do I have to activate something in CubeIDE or in some register to use the SMPS?
Is there something wrong in the design? (PDF)
I put R107 as a jumper to switch between mode 1 and 2 described in datasheet. And none of this modes worked.
Thank you for your help.