STM32H735 debug/flash problem
Hi, I have a board with STM32H735I.
I can only detect the IC when boot0 is tied to 3V3 effectively putting the MCU into DFU bootloader mode. In this mode, I can flash it OK with stlink or even USB-DFU. However, once I tie boot0 to gnd the device won't run correctly. and if I leave it at 3v3 it stays in bootloader mode.
I know someone else has posted about this, but no answers. https://community.st.com/t5/stm32-mcus-boards-and-hardware/stm32h735-problem-flashing-no-contact-to-%C2%B5c-while-boot0-gnd/m-p/570571#M14148
Schematics attached. I figured I must have some pin pulled up instead of down or similar.
thank you