Skip to main content
Visitor II
January 11, 2024
Question

STM32H735DK programming and debuggiing via stlink

  • January 11, 2024
  • 3 replies
  • 3439 views

i've recently purchased STM32H735G DK board. 

When i connect it to PC via USB cable, it screen is showing output as per already programmed code and its working.

power LED (LD5) is green and STlink LED (LD6) is red.

But when ever i try to load a new code to this board, a msg is generated "fatal error st link no mcu found".

i'm unable to resolve the issue.

is it due to some jumper settings? i've kept all the jumper settings as default.

Regards 

    This topic has been closed for replies.

    3 replies

    Technical Moderator
    January 11, 2024

    Hello @NSing.5 ,

    Try to update the ST Link firmware.

    Maybe you missed activate the sys->Debug.

    Try connecting the BOOT pin to VDD.

    NSing.5Author
    Visitor II
    January 14, 2024

    Sir, 

    i've opted for default settings of STM32H735DK developemnt kit.

    And by default from Trace and debug -> Jtag 5pin is selected.

    is there anything additional i've to do.

    i've attached image of settign page (STM32cubeMx) for refrence

    Regards

     

    Technical Moderator
    January 15, 2024

    Try using ''Connect Under Reset'' mode.

    NSing.5Author
    Visitor II
    January 16, 2024

    what is the process to"connect under reset"?

     

    NSing.5Author
    Visitor II
    January 16, 2024

    Try connecting the BOOT pin to VDD.

    how it is to be done, is there any jumper setting?

    Technical Moderator
    January 18, 2024

    Hi @NSing.5 

    I recommend you use latest release of STM32CubeProgrammer, instead of ST-LINK Utility.

    Please follow this article that may help you: Unable to connect to STM32H7 devices - STMicroelectronics Community.

    NSing.5Author
    Visitor II
    January 20, 2024

    sir,

    as suggested i've used STM32cube programmer.

    Now the board is connecting to STM32cube programmer. it is reading memeory and other stuff from the board.

    NSing5_0-1705768866148.png

    i've not erased the memory or programmed it from STM32cube programmer.

    But still when i try to program it from IAR workbench, it is unable to program the board. 

    Graduate II
    January 20, 2024

    Check IAR version and patches for support of H7 parts

    STM32Cube_FW_H7_V1.10.0\Utilities\PC_Software\IDEs_Patches\EWARM\EWARMv8_STM32H72x-73x_Support_V0.2.zip