STM32H745 Dual Core Power Management
I am running FREERTOS on both M7 and M4 on STM32H745 MCU. In general M7 gets booted up and release HSEM for M4 then it will start.
Now my question , if there no activity in M7 (idle mode), would like to keep M4 actively running and put M7 in sleep. Is it possible to keep M7 in sleep and still continue to run M4 to save power ?. If so how to enable this scenario and what is the way to wake up back the M7 ? Should it be again through M4 or it can done from any peripheral interrupt like touch or keys etc ?
Although H7 series is performance device, we are using it in battery based application. Could you suggest best power management options
for D1, D2 and D3 domains under FREERTOS. are there any APIs already for achieving above scenario?