Skip to main content
Visitor II
July 22, 2022
Question

STM32H750XBH6 BGA soldering

  • July 22, 2022
  • 1 reply
  • 1054 views

Hi there.

I got in trouble with H750XBH6.

I designed a costum board base on mcu above.

I followed datasheet recommendations for BGA footprint.

Now I got problem with soldering. The pads are too small and doesn't make connection with chip balls.

So the chip doesn't work properly and I guess there are many of non-connected pins specially on GND and VCC pins under chip.

I got confused about the 0.225mm pad recommendation in datasheet.

Why the pads are smaller than the chip balls?

The balls are about 0.4mm ​

    This topic has been closed for replies.

    1 reply

    Technical Moderator
    October 25, 2022

    Hi @SJaha.2​,

    The spherical shape makes the pads smaller than the diameter of the balls which is compliant with JEDEC standards.