Skip to main content
Graduate II
June 6, 2024
Solved

STM32H755 emmc compatibility - IS22TF08G-JCLA2

  • June 6, 2024
  • 2 replies
  • 1079 views

Hello,

In the RM0399 58.1 it is mentioned that EMMC is supported up to Version 4.51. I want to use the part  IS22TF08G-JCLA2 which supports a number of emmc interfaces up to 5.1 are these parts compatible? 

    This topic has been closed for replies.
    Best answer by KDJEM.1

    Hello @sarun ,

    The HS200 mode supported in IS22TF08G is compatible with STM32H755.

    KDJEM1_1-1718103452213.png

     

    KDJEM1_0-1718103370314.png

    Thank you.

    Kaouthar

    2 replies

    KDJEM.1Answer
    Technical Moderator
    June 11, 2024

    Hello @sarun ,

    The HS200 mode supported in IS22TF08G is compatible with STM32H755.

    KDJEM1_1-1718103452213.png

     

    KDJEM1_0-1718103370314.png

    Thank you.

    Kaouthar

    sarunAuthor
    Graduate II
    June 11, 2024

    Thank you @KDJEM.1  for confirmation