Skip to main content
Visitor II
July 20, 2023
Question

STM32H7B3 No Display

  • July 20, 2023
  • 3 replies
  • 1492 views

Hello;

 

I need your support to resolve an issue with the STM32H7B3.

Today once I connected the board to my PC; I noticed that nothing pops up in the display;; I mean... black screen. 

But ... I can see the green lights over the board on and I'm able to connect it thru the SMT32CubeProgrammer

here is an Image:

maununez_0-1689883260955.png

is connected.

 

What can I do to see graphics over the display?

 

Thanks in advance and your support 

 

 

    This topic has been closed for replies.

    3 replies

    Super User
    July 20, 2023

    Your screenshot shows that the FLASH is erased (0xFF). That means there is no program on the board, so nothing is sending data to the display.

    Is this a STM32H7B3I-DK? You can re-flash the demonstration firmware if you can find it. I can try to look...

    maununezAuthor
    Visitor II
    July 21, 2023

    Thank you TDK | Evangelist for your quick support.

    I'm going to follow your instructions .. I mean re-flash the board

    I'll share the result

     

    Super User
    July 20, 2023
    maununezAuthor
    Visitor II
    July 21, 2023

    Hello Again @TDK 

     

    I did the step; the re-flash, but looks like there is a problem once STM32CubeProgrammer try to delete the external memory

    maununez_0-1689969594640.png

    in the next image; you can see that... I'm trying to upload the demo.hex

     

    maununez_2-1689969862120.png

    and I have as External loader the one which is in the next image:

    maununez_3-1689969963202.png

    In resume: the problem is when then CubeProgrammer is trying to delete External Memory

    Once again, thank you for your support.

    what can I do?

    best regards.

     

     

     

    Technical Moderator
    July 21, 2023

    Hello @maununez, Welcome to ST Community.

     

    Your chip seems to be fully erased. Would you please specify the expected behavior? 

    Flashing the demo would be a good start to test the LCD panel.

     

    maununezAuthor
    Visitor II
    July 21, 2023

    Thank you @FBL for your support

    As @TDK suggested too

    I'll re-flash the board and soon I'll share the result

     

    best regards;