STM32H7B3I-DK Board Issue: Faulty LD7 and No STM32 Target Found
Hi Community,
I am currently facing an issue with my STM32H7B3I-DK board. The board was working fine, but suddenly, while I was uploading the code, the LD7 LED turned on indicating a low voltage fault. However, I am confident that the USB is providing the correct voltage.
In an attempt to resolve the issue, I tried upgrading the firmware and used CubeProgrammer to reset the board with a shown voltage alternating between 0.21v, 0.35v and 0v. I also tried using the STLink utility, but I keep getting the “No STM32 Target found” error, and there is a Fail File existing in the mass storage when connecting the board containing "The interface firmware FAILED to reset/halt the target MCU".
Additionally, I noticed that the WiFi LED (LD1) and the 5V Power LED (LD5) are weakly lit. I am unsure if this is related to the current issue or if it’s a separate problem.
I have been searching for solutions online and tried several suggested methods, but none have worked so far. I would appreciate any help or suggestions on how to resolve these issues.
Troubleshooting Steps Taken:
- Upgraded the firmware.
- Used CubeProgrammer to reset the board.
- Utilized STLink utility to erase memory.
Current Issues:
- LD7 LED indicating low voltage.
- “No STM32 Target found” error.
- Slight lighting of WiFi LED (LD1) and 5V Power LED (LD5).
Board Details:
- Board: STM32H7B3I-DK
- Power Source: USB
I hope it's not a faulty hardware component, I appreciate any assistance!