Skip to main content
Graduate II
March 30, 2022
Question

STM32H7B3I-DK Disco. Using CN12 Segger Pin Header with J-Link

  • March 30, 2022
  • 0 replies
  • 547 views

Hi

I wished to use my Segger J-link Pro to debug my Disco' Board, but when I connect using CN12 the Segger Spring Pin header it won't connect to the target, although the IDE and Programmer can "see" the j-Link probe.

0693W00000LwDfRQAV.png 

I read the board's user manual (UM2569 - Rev 3) and it gave instructions for the use of CN8 the 10 pin mips connector, but not CN12. I assumed that the instructions would apply to both connectors, but using the two methods described i could not get CN12 to work. With the ST-Link processor reset link CN13 closed there wasn't any power going to the CN12 Pins.

Has anyone tried this and have been able to connect?

Regards

Rob

    This topic has been closed for replies.