STM32H7B3I-EVAL: Cannot find connector for their header pins
Hello,
I admit that I feel like I'm missing something obvious here, but I am using the STM32H7B3I-EVAL evaluation board and they have 0.05" pitch header pins for some of their connectors (CN5/CN6). I am trying to source a single position connector that can connect to their header pins (P/N: FTR-130-53-L-D-LC).
I am looking for something similar to the image below, but 1.27mm (or 0.05") pitch and female.
I want single-position so I can send various GPIO signals to different boards. Is anyone aware of a product that can do this?