STM32L031K6 Power Issues SPV1050 (mandatory bulk capacitors)
According to the datasheet a 10uF should be considered at VDD and 1uF at VDDA.
Are these values mandatory for a robust design? I’ve checked various STM32L0 schematics on the internet and most of them use only the 100nF capacitors.
I’m asking this question because I face two issues:
- The LDO from SPV1050 (energy harvester) collapses when I connect the MC including the 10uF capacitor
- I have very less space on the PCB, every component I can omit will help
Additional question:
Can I leave the NRST pin floating and skip the capacitor, when I do not need any reset on my PCB? I suppose the MC has internal pull-up.
Thanks a lot for any feedback!