Skip to main content
Visitor II
December 10, 2015
Question

STM32L152 read memory protection - cannot flash anymore

  • December 10, 2015
  • 1 reply
  • 940 views
Posted on December 10, 2015 at 09:40

Hello

I have a nucleol152 board. As I need to protect a memory area, I used this function to make a read protection + a write protection on zone specific areas:

  __IO uint32_t WPR_Value = 0x0, WriteProtectedPages = 0x0;

  FLASH_Unlock();

  /* Unlock the Option Bytes */

  FLASH_OB_Unlock();

 

  /*Set read protection to 1*/

  FLASH_OB_RDPConfig(OB_RDP_Level_1);

 

  /* Get pages write protection status */

  WPR_Value = FLASH_OB_GetWRP();

 

  /* Get current write protected pages and the new pages to be protected/unprotected */

  WriteProtectedPages = (WPR_Value & FLASH_PAGES_TO_BE_WRITE_PROTECTED);

 

  /* Check if desired pages are not yet write protected */

  if(WriteProtectedPages != FLASH_PAGES_TO_BE_WRITE_PROTECTED)

  {

    /* Enable the pages read/write protection */

    FLASH_OB_WRPConfig(FLASH_PAGES_TO_BE_WRITE_PROTECTED, DISABLE);

 

    /* Generate System Reset to load the new option byte values */

    FLASH_OB_Launch();

  }

 

  /* Lock the Option Bytes */

  FLASH_OB_Lock();

When I try to reflash my board using the stlink, I have a fail. I understand it fails as memory is protected.

I tried several things to unblock the memory:

I use GDB to write the following sequence

unlock flash

(gdb) set {int}0x40023C10 = 0x8C9DAEBF

(gdb) set {int}0x40023C10 = 0x13141516

unlock OB

(gdb) set {int}0x40023C14 = 0xFBEAD9C8

(gdb) set {int}0x40023C14 = 0x24252627

switch to RDP level 0

(gdb) set {int}0x1FF80000 = 0x000000AA

This last operation always fails and GDB returns that it cannot access to this memory area.

I tried to push this sequence into a RAM program but it still has no effect (unless the code I downloaded is not working well).

I saw this type of topic and I was wondering if it was the only solution to unblock my memory.

http://www.mobilewill.us/2015/06/stm32-nucleo-and-dfu-usb-bootloading.html

Could you tell me how I should proceed to unblock the memory?

Thanks for your support

#rdp #nucleo #st-link #swd
    This topic has been closed for replies.

    1 reply

    Visitor II
    June 1, 2018
    Posted on June 01, 2018 at 11:37

    Hey are you getting a solution of this issue??