Skip to main content
Visitor II
March 20, 2018
Question

STM32L1xx can't write to internal EEPROM after being programmed with ST-Link

  • March 20, 2018
  • 2 replies
  • 1897 views
Posted on March 20, 2018 at 08:55

Hello,

I've encountered a systematic problem with the STM32L151 which I'm finding hard to debug.

We write a bootloader and main image to the flash memory using the ST-Link CLI, and at the same time write some individual configuration data to the internal EEPROM memory. The command usually looks something like this :

C:\Program Files (x86)\STMicroelectronics\STM32 ST-LINK Utility\ST-LINK Utility\ST-LINK_CLI.exe -c

-w32 0x8080000 0xaf000c -w32 0x8080004 0x18 -w32 0x8080498 0x0 -w32 0x80804a0 0x0

-P firmwares\bootloader-v1.3.hex -P firmwares\firmware-v0.8.12.hex

-V after_programming -Q 1>&2

All four operations complete successfully, and after a reset, everything performs as expected (this is what we've been doing on thousands of devices). In some cases though, the MCU gets reprogrammed in-system and it doesn't get powered down before use. It then remains powered on 24/7. The problem here is that in this state, the MCU is unable to write to its own internal EEPROM unless we force a reset. (after that, it works fine).

Obviously, the simple solution is 'do a reset after programming them', but I'd like to know what's actually causing this, since I'm pretty sure some systems are getting stuck in this state on their own, regardless of how they were programmed initially. Is there something in the MCU registers that indicates that the EEPROM is badly initialized, or something like that? Or should I do a test read-modify-check on boot and reset the MCU if that fails?

I'm using the StdPeriph library, v1.3.1 and calling DATA_EEPROM_Unlock() before every write, and DATA_EEPROM_Lock() when finished.

#stm32l1 #st-link #stm32l1-eeprom-nvm
    This topic has been closed for replies.

    2 replies

    Visitor II
    March 20, 2018
    Posted on March 20, 2018 at 09:59

    Update with more information: I can't replicate the bug with the debugger attached, since the bug appears during programming, but I dumped the contents of the FLASH SFRs to UART in both cases.

    The difference when the writes fail is that the WRPERR bit is set in the FLASH->SR register even before I attempt to write to the EEPROM. Is it possible that my ST-Link command above is causing a Write Protection error by writing to a wrong address? (as far as I can tell, all the writes succeed, and the addresses are 32-bit aligned)

    Visitor II
    March 20, 2018
    Posted on March 20, 2018 at 12:01

    Second update:

    The problem seems to be occurring within a loop where we do something like this: (simplified a little by replacing some constants and structs)

    // EEPROMTableStart refers to an array in a struct, it starts at 0x8080114 uint32_t zeroes = 0;

    uint8_t i, j, status;

    for (j = 0; j < 68; j++) {

      for (i = 0; i < 3; i++) {

        status = DATA_EEPROM_ProgramWord((uint32_t) (&EEPROMTableStart[j])+(i*4), zeroes);

        if (status != FLASH_COMPLETE) {

          return ERROR; // <<< Problem here, status == FLASH_ERROR_WRP with j = 4

        }

      }

    }

    The strange part (to me) is that this loop fails, not on the first iteration, but on the fourth, writing to 0x8080144.

    But this ONLY happens when I've just erased the EEPROM using the ST-Link :

    ST-LINK_CLI.exe -c -SE ed1 -Q

    When I do this, the program will return an ERROR, on the first boot. All subsequent boots are fine. Call the EEPROM erase command above, error. Reset MCU, no error. 

    If I have the debugger connected, it doesn't always fail, but if not, it fails systematically on the first boot after an EEPROM erase.

    Visitor II
    March 22, 2018
    Posted on March 22, 2018 at 11:37

    I ended up fixing the problem : during the long loop of writing to the EEPROM, we had an interrupt that was performing a write to EEPROM, and locking it after it was done.