Question
STM32l412 Nucleo-32 Dev Board has shorted pins?
The following pins appear to be shorted on the STM32L412 Nucleo-32 Dev Board :
A4 (PA5) shorted to D4 (PB7)
and
A5 (PA6) shorted to D5 (PB6)
Is it possible someone can verify, I have checked four Nucleo-32 boards and all show the shorted pins. The Nucleo board also does show this shorted behavior when powered up in the system.