Skip to main content
Visitor II
February 11, 2022
Question

STM32L431 DAC

  • February 11, 2022
  • 2 replies
  • 2355 views
    This topic has been closed for replies.

    2 replies

    Technical Moderator
    February 11, 2022

    Welcome, @kazuchib​, to the community!

    R-2R networks are also called resistor networks and DACs also like to use this R-2R.

    Where do you see a difference?

    Regards

    /Peter

    kazuchibAuthor
    Visitor II
    February 11, 2022

    Thank you for your answer

    I thought the resistor strings were the method of linking below.

    https://www.researchgate.net/figure/Simplest-Voltage-Output-Thermometer-DAC-The-Kelvin-Divider-String-DAC_fig1_266008269

    Can you show me the details of the DAC used in the STM32L431?

    Technical Moderator
    February 11, 2022

    May I ask what this information is relevant for?

    Background: with the R-2R converter, the binary value is fed in directly and then decoupled with a voltage follower, so that the R-2R network is not visible to the outside world. But the principle corresponds to what can also be seen in the Wikipedia article mentioned above.

    Regards,

    /Peter

    kazuchibAuthor
    Visitor II
    February 13, 2022

    I am making an application that changes voltage very quickly.

    I replaced the microcomputer of another company with this microcomputer.

    Even in previous applications, there was a temporary strange behavior when changing the voltage at high speed.

    In the previous application, I thought about the correction method from the design information.

    I would like to consider making corrections from the design information this time as well.

    Technical Moderator
    February 14, 2022

    OK, for timing problems with fast signals the internal setup is irrelevant, because the timing behavior of the whole DAC block and its possible error limits are listed in the datasheet, section 6.3.19.

    Does it answer your question?

    Regards

    /Peter

    kazuchibAuthor
    Visitor II
    February 18, 2022

    Sorry for the late reply.

    Thank you for your answer.

    I will proceed with the verification based on this material and the behavior of R-2R.

    Best regards.