STM32L476 + STLINK2 SWD => overconsumption
Hello,
I have a STM32L476 board. This board consumes 4µA.
When I reprogram the board by SWD from TrueStudio, after deconnecting the STLINK2, the board consumes 800µA. If I reset the board, the current consumption is still 800µA, which is not acceptable for a battery product. The only way to have a normal current consumption (4µA) is to remove the battery, wait the condensators to discharge then re-solder the battery.
Is there another tool which permit to program the STM32L476 without producing this current overconsumption?
It is a real problem to always unsolder-wait-resolder the battery.
Best regards
Mich