STM32L476G-EVAL X1 not oscillating for RTC LSE use
Hello,
I have an STM32l476G evaluation board. I've configured the CubeMX project to enable the RTC to be run from the 32KHz LSE crystal which should be X1 on the board. However, when putting an oscilloscope on the x1 pins, I do not see any oscillation coming from the pins. I'm not sure if there's a jumper, or bridge I need to change on the board, as I can't find the schematic for the evaluation board online. PC14 and PC15 does not oscillate as well, which is expected as I can't see anything coming from the crystal.