STM32L4A6VG 3.3V breakdown
Hi everyone,
I designed a custom board and now I found two MCUs (STM32L4A6VG) are breakdown. The MCU is running at 3.3V and all VDD, VDDA, VREF+, VDDUSB and VBAT is connected to the same 3.3V source. Here's what I found.
For the initial trial, I did 2 boards and one became very hot at MCU after running for several days. The resistance between 3.3V and GND is around 10 ohms. The MCU can still run even it is very hot.

For the second trial, I change the TVS at 12V input and the clamp voltage is 14V. This time I did 7 boards and one failed to run just after powering on. The resistance between 3.3V and GND is around 80k ohms. I removed the LDO and the resistance dropped to around 30k ohms. I applied 3.3V using an independent power source and the current was over 600mA (voltage is 1.8V so there's not enough power. Using higher current may destroy the MCU completely). Now the resistance between 3.3V and GND is around 400 ohms.

Any suggestion is welcomed.
Best,
SL61