Skip to main content
Visitor II
April 22, 2021
Question

STM32L552 SMPS hardware design

  • April 22, 2021
  • 2 replies
  • 1123 views

I have a question about connecting of the SMPS V15SMPS pins. From the datasheet we see, that the V15SMPS_1 and V15SMPS_2 pins are connected internaly. But, on the "Figure 6. SMPS step down converter power supply scheme" they are alco connected externally.

So, the question is: should I externally connect V15SMPS_1 and V15SMPS_2 pins on my PCB or not.

    This topic has been closed for replies.

    2 replies

    Visitor II
    April 22, 2021

    Hello

    One of the reasons that power pins are multiple is to well distribute flowing currents on silicon chip.

    IMO both pins must be connected.

    Visitor II
    April 23, 2021

    Hi Dmytro Medvid,

    V15SMPS_1 and V15SMPS_2 pins are already connected internally in the chip.

    For the PCB, you should connect these pins externally.

    Please refer to the AN5211 for more details (p33/40).

    0693W00000AMM9JQAX.pngBest Regards,

    Ons.